ScriptDeviceRepository

class

ScriptDeviceRepository.

ScriptDeviceRepository

Bases: object

Device respository.

sources

Get the repository sources of the device repository.

create_device_identification

type

id

version

Factory method for an DeviceId object.

Parameters
  • type (int) -- The device type.

  • id (str) -- The device id.

Return type

str

Returns

A new DeviceId object with the provided values.

create_module_identification

type

id

version

module_id

Factory method for an ModuleId object.

Parameters
  • type (int) -- The device type.

  • id (str) -- The device id.

  • module_id (str) -- The module id.

Return type

str

Returns

A new ModuleId object with the provided values.

import_device

source

stream=None

path=None

source_path=None

save_device_cache=True

converter_factory_guid=None

Import a device description file into a repository.

 WARNING

The original C# function that is called with this method contains 3 overloads. It is strongly advised to pass all arguments with their respective keywords. stream, path, and source_path are not actually optional, they just aren't required in every overload. Pass them if your overload needs them!

import_device(stream, source, source_path, save_device_cache=True) (1/3)

Parameters
  • stream (System.IO.Stream) -- The stream that contains the device description. This must be a valid device description file. Other types of device descriptions must be imported by special plug-ins.

  • source (ScriptRepositorySource) -- The repository source where the device should be stored. This parameter may be None, in which case the default repository source is used. The repository source must be one of the sources defined in sources.

  • source_path (str) -- Sourcepath for the import. Relative file references inside the device description are resolved relative to this source path. May be empty, if the device description contains only absolute file references.

  • save_device_cache (bool) -- If True, after removing the device the device cache is also written. If False, the device cache is not written. If many devices are removed, this is much faster.

Return type

DeviceId

Returns

The ID of the imported device description.

import_device(path, source, save_device_cache=True) (2/3)

Import a device description file into a repository.

Parameters
  • path (str) -- The file that contains the device description. This must be a valid device description file. Other types of device descriptions must be imported by special plug-ins.

  • source (ScriptRepositorySource) -- The repository source where the device should be stored. This parameter may be None, in which case the default repository source is used. The repository source must be one of the sources defined in sources.

  • save_device_cache (bool) -- If True, after removing the device the device cache is also written. If False, the device cache is not written. If many devices are removed, this is much faster.

Return type

DeviceId

Returns

The ID of the imported device description.

import_device(path, source, converter_factory_guid, save_device_cache=True) (3/3)

Convert a foreign device description file and import the result into a repository.

List of known converter factories:

{C633F245-876F-45E8-AAB4-3FBD994C08B8}

Use as default because all available converters are tried

{3992C588-7BDB-4A7C-908D-F444808D8CD2}

XML files of EtherCAT

{6066AEF4-F19A-41ac-A249-721BDAE32D40}

GSDML files of Profinet IO

{CDDE0374-9EFD-401e-93C8-F19443FB60ED}

XML files of Sercos3

{1ce4a9c1-37d3-496c-9e80-cd99ad3807ee}

EDS files of CANbus

Parameters
  • path (str) -- The file that contains the device description. This must be a valid device description file. Other types of device descriptions must be imported by special plug-ins.

  • source (ScriptRepositorySource) -- The repository source where the device should be stored. This parameter may be None, in which case the default repository source is used. The repository source must be one of the sources defined in sources.

  • converter_factory_guid (str) -- The guid of the converter to import a foreign device description. For example CANopen EDS files.

  • save_device_cache (bool) -- If True, after removing the device the device cache is also written. If False, the device cache is not written. If many devices are removed, this is much faster.

Return type

DeviceId

Returns

The ID of the imported device description.

import_vendor_description

source

stream=None

path=None

source_path=None

Import a device description file into a repository.

 WARNING

The original C# function that is called with this method contains 2 overloads. It is strongly advised to pass all arguments with their respective keywords. stream, path, and source_path are not actually optional, they just aren't required in every overload. Pass them if your overload needs them!

import_vendor_description(stream, source, source_path) (1/2)

Parameters
  • stream (System.IO.Stream) -- The stream that contains the vendor description. This must be a valid vendor description file. Other types of vendor descriptions must be imported by special plug-ins.

  • source (ScriptRepositorySource) -- The repository source where the device should be stored. This parameter may be None, in which case the default repository source is used. The repository source must be one of the sources defined in sources.

  • source_path (str) -- Sourcepath for the import. Relative file references inside the vendor description are resolved relative to this source path. May be empty, if the vendor description contains only absolute file references.

Return type

ScriptVendorDescription

Returns

The imported vendor description.

import_vendor_description(path, source) (2/2)

Parameters
  • path (str) -- The file that contains the vendor description. This must be a valid vendor description file.

  • source (ScriptRepositorySource) -- The repository source where the device should be stored. This parameter may be None, in which case the default repository source is used. The repository source must be one of the sources defined in sources.

Return type

ScriptVendorDescription

Returns

The imported vendor description.

remove_device

device_id

source

save_device_cache=True

Remove a device from the specified repository source.

Parameters
  • device_id (DeviceId) -- Defines the device to remove.

  • source (ScriptRepositorySource) -- Remove the device from this repository source. If None the device is removed from the default repository source.

  • save_device_cache (bool) -- If True, after removing the device the device cache is also written. If False, the device cache is not written. If many devices are removed, this is much faster.

remove_vendor_description

vendor_id

source

Remove a vendor description from the specified repository source.

Parameters
  • device_id (int) -- The vendor id.

  • source (ScriptRepositorySource) -- Remove the device from this repository source. If None the device is removed from the default repository source.

save_device_cache

Saves the current devices in the device cache. Could be used to force it after adding or removing many devices.

rebuild_device_cache

Rebuild the device cache.

The device cache is deleted, initialized and saved.

get_device_category

category_id

This overload is called when category_id is of type int.

Get the device category with the specified device category ID.

Parameters

category_id (int) -- The device category ID of the device category implementation. This value corresponds to the DeviceDescription/DeviceInfo/Category tags of the device description file.

Return type
Returns

The requested device category, or None if the device category does not exist.

This overload is called when category_id is of type Guid:

Get the device category with the specified type GUID.

Parameters

category_id (Guid) -- The type GUID of the device category implementation.

Return type
Returns

The requested device category, or None if the device category does not exist.

get_device_family

family

Device family.

Parameters

family (str) -- VendorID:FamilyID.

Return type

ScriptDeviceFamily

get_all_devices

name=None

device_id=None

source=None

Get a collection containing all devices in the repository.

 WARNING

The original C# function that is called with this method contains 5 overloads. It is strongly advised to pass all arguments with their respective keywords.

get_all_devices() (1/5)

Devices which are installed in more than one repository source are returned only once.

Returns

A device collection containing the current result of the query.

get_all_devices(device_id) (2/5)

Get a collection containing all devices in the repository, including local modules of device_id

Parameters

device_id (DeviceId) -- The id of the device that provides the context for the local modules.

Returns

A device collection containing the current result of the query.

get_all_devices(source) (3/5)

Get a collection containing all devices in the specified repository source.

Parameters

source (ScriptRepositorySource) -- The repository source to enumerate.

Returns

A device collection containing the current result of the query.

get_all_devices(device_id, source) (4/5)

Get a collection containing all devices in the specified repository source.

Parameters
  • device_id (DeviceId) -- The id of the device that provides the context for the local modules.

  • source (ScriptRepositorySource) -- The repository source to enumerate.

Returns

A device collection containing the current result of the query.

get_all_devices(name, source=None) (5/5)

Get all device which contain the specified name.

Parameters
  • name (str) -- Text which the name of the device has to contain.

  • source (ScriptRepositorySource) -- If not None, only this repository source will be searched.

Return type

tuple

Returns

A device tuple containing the current result of the query.

get_all_vendor_descriptions

source=None

Get a collection of all vendor descriptions in the repository.

 WARNING

The original C# function that is called with this method contains 2 overloads. It is strongly advised to pass all arguments with their respective keywords.

get_all_vendor_descriptions() (1/2)

Return type

PythonTuple

Returns

A collection of vendor descriptions.

get_all_vendor_descriptions(source) (2/2)

Get the vendor description with the specified vendor Id.

Parameters

source (ScriptRepositorySource) -- Repository source.

Return type

PythonTuple

Returns

A collection of vendor descriptions containing the current result of the query.

get_vendor_description

vendor_id

Get the vendor description with the specified vendor Id.

Parameters

vendor_id (int) -- Vendor Id.

Returns

The requested vendor description, or None if the vendor description does not exist.

class

ScriptDeviceRepository.

ScriptRepositorySourceList

Bases: list

A collection of ScriptRepositorySource objects.

add

name

location_url

Add a new repository source with the specified name.

Parameters

name (str) -- Name for the new source.

Returns

The added repository source.

remove

source

Remove an existing repository source.

Internal sources cannot be removed.

Parameters

source (ScriptRepositorySource) -- The repository source to remove.

move

source

index

Move an existing repository source to the specified location in the collection.

Parameters
  • source (ScriptRepositorySource) -- Existing repository source.

  • index (int) -- New index of the repository source.

class

ScriptDeviceRepository.

ScriptRepositorySource

Bases: object

Repository source.

name

Get or set the name of the repository source.

Return type

str

location_url

Get or set the location URL.

Return type

str

is_internal

Return whether the repository source is internal.

If true, then this repository source is an implicit source (like the project internal repository or the installation specific repository). Therefore its properties like name and location are readonly and may not be changed.

Return type

bool

class

ScriptDeviceRepository.

ScriptDeviceCategory

Bases: object

Category of devices.

Devices can be grouped into categories by means of the DeviceDescription/Device/DeviceInfo/Category tags of the device description file. One can implement a corresponding class of this interface to display these types in a user-friendly way.

category_id

Id of the category.

Return type

int

parent_category

The type GUID of the parent device category implementation, or Guid.Empty, if this device implementation is top-level.

Return type

Guid

name

Gets a user-friendly display name for this device category.

This string should be localized.

Return type

str

description

Gets a user-friendly description for this device category.

This string should be localized.

Return type

str