SysDirOpen (FUN)

FUNCTION SysDirOpen : RTS_IEC_HANDLE

Opens a specified directory and returns a handle and the first directory entry.

szDirEntry is expected to provide enough space to write the direcory entry to.

In case szDirEntry is 0, the first directory entry may be retrieved with SysDirRead.

InOut:

Scope

Name

Type

Comment

Return

SysDirOpen

RTS_IEC_HANDLE

Returns the runtime system error code (see CmpErrors.library)

Input

szDir

REFERENCE TO STRING

Name of directory.

Note

Empty string ('') is the request for the current working directory.

szDirEntry

REFERENCE TO STRING

OUT_PARAMETER, optional: Directory entry as string, may be 0

diMaxDirEntry

DINT

OUT_PARAMETER, optional: Max number of bytes to write in pszDirEntry

pDirInfo

POINTER TO DirInfo

OUT_PARAMETER, optional: Directory information, may be 0

pResult

POINTER TO RTS_IEC_RESULT

OUT_PARAMETER: Pointer to runtime system error code (see CmpErrors.library)