Example Description

 

Overview

Short Description

The EcoStruxure Machine Expert project AltivarPLCopenEtherNetIPExample.project implements an application example which shows how to implement an Altivar variable speed drive controlled via fieldbus EtherNet/IP. The application example is based on a programming framework supporting general machine control. The monitor and control functions for the Altivar drives are implemented using the PLCopen function blocks from the library GMC Independent PLCopen MC.

System Requirements and Limitations

The application example has been created with the components listed in the table:

Component

Type and Version

Software

EcoStruxure Machine Expert V1.1

Controller

TM251MESE1)

Additional devices

oAltivar 320, equipped with the communication module VW3A3616

oAltivar 340E (Ethernet embedded)

oAltivar 630, equipped with the communication module VW3A3720

oAltivar 930 (Ethernet embedded)

1)   This example is based on the Modicon M251 Logic Controller, however, in principle, the concepts for the implementation of the Altivar drives on EtherNet/IP are the same for other EcoStruxure Machine Expert controllers. As a precondition, the controller must support the EtherNet/IP  scanner and the GMC Independent PLCopen MC library.