GetBaudrate (FUN)

FUNCTION GetBaudrate : UINT

This function returns the current baudrate of the bus. Information can be also read by GetDiagnosis.

InOut:

Scope

Name

Type

Comment

Return

GetBaudrate

UINT

baudrate in kBit/s

Input

hDriver

CAA.HANDLE

handle of CAN interface

peError

POINTER TO ERROR

optional pointer to error enum