BUS_STATE (ENUM)

TYPE BUS_STATE :

This enumeration lists all possible states of a fieldbus. The mapping to the according fieldbus specific states is defined by the associated fieldbus stack.

Attributes:

qualified_only

InOut:

Name

Comment

UNKNOWN

The bus state is unknown.

STOPPED

The fieldbus is stopped. No I/O transfer can be processed.

RUNNING

The fieldbus is running.

ERROR

The fieldbus is in error state. GetBusError supplies the specific error code.

DISABLED

Bus is disabled in device tree.