PN_ADDR (STRUCT)

TYPE PN_ADDR : STRUCT

data structure for physical/native identification or subslot of a PROFINET IO Device.

InOut:

Name

Type

Initial

Comment

VERSION

BYTE

1

Version of the data structure (1= Version 1)

MASTER

BYTE

D

PN_DEVICE_ID

Identification of the Field Device

API

DWORD

application process identifier

SLOT

WORD

Slot Number (identification of a slot)

SUBSLOT

WORD

Subslot Number (identification of a subslot)