FUNCTION_BLOCK LCon EXTENDS BehaviourModelBase IMPLEMENTS ILCon
Base implementation of a PLCopen Level Controlled Behavior Model (see: ILCon)
For use, this block should be extended and the specific inputs and outputs must be supplemented. The output eErrorID of the application-specific enum type ERROR must be added.
| InOut: |
|