PBSlaveDiag.Enable (PROP)

PROPERTY Enable : BOOL

This property returns if the node is enabled in the device tree. The setter can be used to change the Enabled flag. If enabling/disabling is not supported on the node the flag’s value will not change.