METHOD UpdateConfiguredBaudrate : UDINT
Change the configured baud rate of the master configuration.
Only possible if the profibus master is disabled (see DED.Reconfigure function block).
Scope
Name
Type
Return
UpdateConfiguredBaudrate
UDINT
Input
Baudrate
ProfibusBaudrate