AdapterDiagnosis (FB)

FUNCTION_BLOCK AdapterDiagnosis

Gets the diag. info of the given IoDrvEtherNetIPAdapter.

InOut:

Scope

Name

Type

Comment

Input

pEtherNetIPAdapter

POINTER TO IoDrvEtherNetIPAdapter

The IoDrvEtherNetIPAdapter from which the diag. info is needed.

Output

uiConnectedModules

UINT

Number of modules connected at the adapter

uiEstablishedClass1Connections

UINT

Number of currently successfull established connections

udiConnectionTimeouts

UDINT

Number of connection timeouts since the adapter started

udiForwardOpenRequests

UDINT

Total number of forward open requests processed by the adapter

udiForwardOpenFails

UDINT

Number of unsuccessfull forward open requests