METHOD GetRecipeNames : DWORD
Returns the recipe names from the corresponding recipe definition
Example:
We have 50 recipes. We want to create a table which shows 10 recipe names at the same time. We define a string array strArr: ARRAY[0..9] OF STRING;
Corresponding to the iStartIndex we can get the recipe names from a specific area.
StartIndex := 0; The names 0..9 are returned.
iStartIndex := 20; The names 20..29 are returned.
In this example:
iSize := 10;
InOut: |
|