The hexadecimal diagnostic codes listed here are output as WORD data type at the DiagCode output of the function block.
|
Code (hex) |
Description |
Options for remedy |
|---|---|---|
|
0000 |
The safety-related function block is not activated (Activate = FALSE). |
Activate the function block by switching Activate to TRUE. |
|
8000 |
The function block is in a normal operating state (S_EDM_Out = SAFETRUE). |
In case of an unexpected combination at the function block inputs relative to the physical input of the sensors, verify S_OutControl and the connected hardware. |
|
8001 |
The start-up inhibit is specified with S_StartReset = SAFEFALSE. |
Removal of the start-up inhibit with a positive edge at Reset. |
|
8010 |
The S_OutControl input is SAFEFALSE. |
To switch S_EDM_Out to SAFETRUE, S_OutControl must be SAFETRUE. |
|
C001 |
The start-up inhibit is specified with S_StartReset = SAFEFALSE and Reset is permanently TRUE incorrectly. |
Reset must be FALSE. Verify the reset control device and its wiring. |
|
C010 |
When controlling the contactors with S_OutControl = SAFETRUE, the feedback signal S_EDM1 was indeterminable. S_EDM1 = SAFEFALSE was detected. |
|
|
C011 |
There are two possible causes for this error:
|
|
|
C020 |
When controlling the contactors with S_OutControl = SAFETRUE, the feedback signal S_EDM2 was indeterminable. S_EDM2 = SAFEFALSE was detected. |
|
|
C021 |
There are two possible causes for this error:
|
|
|
C030 |
When controlling the contactors with S_OutControl = SAFETRUE, the feedback signals S_EDM1 and S_EDM2 were indeterminable. S_EDM1 = SAFEFALSE and S_EDM2 = SAFEFALSE was detected. |
|
|
C031 |
There are two possible causes for this error:
|
|
|
C040 |
The connected contactors are not controlled. Once the time specified at MonitoringTime had elapsed, the feedback signal S_EDM1 was indeterminable. S_EDM1 = SAFEFALSE was detected. |
|
|
C041 |
An error was detected once the time specified at MonitoringTime elapsed. There are two possible error causes:
|
|
|
C050 |
The connected contactors are not controlled. Once the time specified at MonitoringTime had elapsed, the feedback signal S_EDM2 was indeterminable. S_EDM2 = SAFEFALSE was detected. |
|
|
C051 |
An error was detected once the time specified at MonitoringTime elapsed. There are two possible error causes:
|
|
|
C060 |
The connected contactors are not controlled. Once the time specified at MonitoringTime had elapsed, the feedback signals S_EDM1 and S_EDM2 were indeterminable. S_EDM1 = SAFEFALSE and S_EDM2 = SAFEFALSE was detected. |
|
|
C061 |
An error was detected once the time specified at MonitoringTime elapsed. There are two possible error causes:
|
|
|
C070 |
The connected contactors were controlled. Once the time specified at MonitoringTime had elapsed, the feedback signal S_EDM1 was indeterminable. S_EDM1 = SAFETRUE was detected. |
|
|
C071 |
The connected contactors are controlled. Once the time specified at MonitoringTime had elapsed, the feedback signal S_EDM1 was indeterminable. S_EDM1 = SAFETRUE was detected. At the same time, a permanent TRUE was detected at Reset. |
|
|
C080 |
The connected contactors were controlled. Once the time specified at MonitoringTime had elapsed, the feedback signal S_EDM2 was indeterminable. S_EDM2 = SAFETRUE was detected. |
|
|
C081 |
The connected contactors are controlled. Once the time specified at MonitoringTime had elapsed, the feedback signal S_EDM2 was indeterminable. S_EDM2 = SAFETRUE was detected. At the same time, a permanent TRUE was detected at Reset. |
|
|
C090 |
The connected contactors were controlled. Once the time specified at MonitoringTime had elapsed, the feedback signals S_EDM1 and S_EDM2 were indeterminable. S_EDM1 and S_EDM2 = SAFETRUE was detected. |
|
|
C091 |
The connected contactors are controlled. Once the time specified at MonitoringTime had elapsed, the feedback signals S_EDM1 and S_EDM2 were indeterminable. S_EDM1 and S_EDM2 = SAFETRUE was detected. At the same time, a permanent TRUE was detected at Reset. |
|
|
C111 |
The function block has detected a simultaneous signal change from FALSE to TRUE at S_OutControl and Reset. |
|