Specification of the maximum permissible response time of the connected contactors.
Data type: TIME
Initial value: #0ms
Connection: Connect this input to a time literal, i.e., to a constant of the data type TIME.
Once the S_EDM_Out output switches to SAFETRUE, the feedback signal at the S_EDM1 and S_EDM2 inputs must become SAFEFALSE within the response time specified here. Otherwise, the function block outputs an error message (output Error = TRUE) and the S_EDM_Out output switches to the defined safe state (SAFEFALSE).
The process of switching off the connected contactors is also time-monitored: if the S_EDM_Out output switches from SAFETRUE to SAFEFALSE, the switching operation of the contactors is also monitored. The feedback signal at the S_EDM1 and S_EDM2 inputs must become SAFETRUE within the permissible response time set at MonitoringTime.
WARNING | |
---|---|