State-controlled input for activating the function block.
Data type: BOOL
Initial value: FALSE
Connection: With TRUE constant or TRUE/FALSE input signal.
Connecting the Activate input to an input signal makes it possible to switch off specific safety-related functions in a targeted manner (e.g., individual areas of machines and systems with a modular construction).
The function block is deactivated when Activate = FALSE. Deactivated function blocks switch their outputs to the defined safe state. S_EquivalentOut = SAFEFALSE and Error = FALSE signals that no error has been detected.
Application examples and information on how to carry out individual deactivation, group deactivation or how to set up modular safety equipment using function block activation can be found in "Activating functionblocks".
Value |
Description |
---|---|
TRUE |
The function block is activated, the inputs are evaluated, and the outputs switched accordingly. Refer to the hazard message below this table. |
FALSE |
The function block is not activated. The S_EquivalentOut output is switched to SAFEFALSE. |
WARNING | |
---|---|