This input is used to specify the start-up inhibit after the Safety Logic Controller has been started up or after the function block has been activated.
When a start-up inhibit is active, all safety-related outputs of the function block are in the defined safe state. This ensures that a machine/system cannot be started up inadvertently. If a start-up inhibit is active, a reset signal is required to remove the inhibit and enable the machine/system to function.
Data type: SAFEBOOL
Initial value: SAFEFALSE
Connection: Connect this input to a variable or constant.
If Activate = TRUE, the possible values at S_StartReset lead to the following function block behavior:
|
Value |
Description |
|---|---|
|
SAFETRUE |
No start-up inhibit for the function block after the Safety Logic Controller has been started up and after the function block has been activated. If no start-up inhibit has been specified for the function block, the SAFETRUE status at the S_GuardLock input can cause the S_GuardLocked output to immediately switch to SAFETRUE. Refer to the first hazard message below this table. |
|
SAFEFALSE |
Active start-up inhibit after the Safety Logic Controller has been started up and after the function block has been activated. The active start-up inhibit must be manually removed by means of a reset signal at the Reset input. Removing the start-up inhibit by means of a positive signal edge at the Reset input can cause the S_GuardLocked output to switch to SAFETRUE immediately (depending on the status of the other inputs). Refer to the second hazard message below the table. |
| WARNING | |
|---|---|
| WARNING | |
|---|---|
The start-up inhibit must only be deactivated (S_StartReset = SAFETRUE) if it is certain that starting up the machine/system will not lead to a hazardous situation or that a suitable start-up inhibit is in place at another location or using other means.
| WARNING | |
|---|---|
| WARNING | |
|---|---|
| WARNING | |
|---|---|