Output for the unlock signal for the guard locking on the safety equipment.
The signal depends on the unlock request present at the UnlockRequest input and on the defined safe state status of the zone of operation (S_SafetyActive input).
Data type: SAFEBOOL
Connection: Connect the S_UnlockGuard output to an interlocking device (e.g., coil of the guard locking) connected to the Safety Logic Controller, either directly or via other safety-related functions/function blocks.
|
Value |
Description |
|---|---|
|
SAFETRUE |
There is a request to unlock the guard locking on the safety equipment. The following conditions must be met:
|
|
SAFEFALSE |
There is no request to unlock the guard locking on the safety equipment, i.e., the interlock is maintained. Reasons:
|
The S_UnlockGuard signal may only switch to SAFETRUE if the zone of operation unlocked in this way is in the defined safe state.
| WARNING | |
|---|---|