Activating function blocks (Activate)

Each safety-related function block can be activated and deactivated via the Activate input.

This means the Activate input can be used to connect/disconnect one or more items of safety equipment and implement modular safety equipment.

If a function block is deactivated (Activate input = FALSE), any state changes and detected edges at its other inputs have no effect on the states of the function block outputs.

NOTE:

In order to activate a function block perpetually, you can connect its Activate input to the TRUE constant.

The topic is explained in terms of the following categories: