SMC_DetermineCuboidBearing (FB)

FUNCTION_BLOCK SMC_DetermineCuboidBearing

This function block will determine the position of a cuboid (corner mark, edge alignment) in the space in dependence of 6 (3/2/1) points given:

For detailed information of transformation modules see the survey on Coordinate Transformations.

InOut:

Scope

Name

Type

Initial

Comment

Input

A1

SMC_Vector3D

First of three points that are located on the surface A of a cube and do not lie on a common line.

A2

SMC_Vector3D

Second of three points that are located on the surface A of a cube and do not lie on a common line.

A3

SMC_Vector3D

Third of three points that are located on the surface A of a cube and do not lie on a common line.

B1

SMC_Vector3D

First of two points that are located on another cube surface B adjacent to A. The projection of this point on surface A may not coincide with the projection of B2.

B2

SMC_Vector3D

Second of two points that are located on another cube surface B adjacent to A. The projection of this point on surface A may not coincide with the projection of B1.

C1

SMC_Vector3D

Point on a further cube surface adjacent to A and B

Output

M

SMC_Vector3D

Common corner point of cube surfaces A, B and C

vAB

SMC_Vector3D

Unit vector on edge line between A and B with start point M

vBC

SMC_Vector3D

Unit vector on edge line between B and C with start point M

vCA

SMC_Vector3D

Unit vector on edge line between A and C with start point M

bError

BOOL

Signals, that an error has occurred within the function block

nError

WORD

0

Error description:

  • 0: No error (bError=FALSE)

  • 1: A1,A2,A3 lie on common line

  • 2: Projections of B1 and B2 on surface A coincide