SMC_OutQueueIsSyncing (FUN)

FUNCTION SMC_OutQueueIsSyncing : BOOL

Returns whether the queue is syncing, i.e. if it is to be emptied completely before being refilled. This is done if a G75 command is issued, which is stored as a m-function with m-value -2.

task-safety: may be called from both tasks

InOut:

Scope

Name

Type

Return

SMC_OutQueueIsSyncing

BOOL

Input

poq

POINTER TO SMC_OUTQUEUE