General Information on the TwidoEmulationSupport Library

 

General Information on the TwidoEmulationSupport Library

Conversion of Function Blocks

The following options are provided for the conversion of function blocks:

oThe function block is converted to a type that already exists in EcoStruxure Machine Expert, for example the function block exists in the standard library.

For more information on standard libraries, refer to the online help CoDeSys Libraries/ Standard Library.

oA new function block that is fully compatible with EcoStruxure Machine Expert - Basic is implemented and part of the TwidoEmulationSupport library.

oFor functions and function blocks that are not intended to be used in a EcoStruxure Machine Expert project, the converter can generate a type with no implementation.

For more information on the conversion of function blocks, refer to Converting EcoStruxure Machine Expert - Basic and Twido Projects.