FUNCTION GetLocalDateTime : ULINT
Related to TimeZone in tzTimeZone this function returns the current date and time in milliseconds since Thursday, 1.1.1970 00:00:00.000, managed in a 64 Bit data type
The default IDateTimeProvider implementation (DateTimeProvider) is in use
| InOut: |