The CODESYS Security Agent is an add-on product for CODESYS. It simplifies the configuration and control of security-relevant aspects in the development system.
At this time, you can configure and create certificates of the controller with the CODESYS Security Agent. After installation, a new Device tab is added to the Security Screen view in the development system. You can then configure encrypted communication with the controller, as well as encrypt the boot application, download, and online change.
A description of the standard security functions in CODESYS Development System are located in the CODESYS Help under the keywords "security", "encryption", and "security screen".
See also