Command 'Step suppression'

Symbol:

Function: This command activates and deactivates the step suppression.

Call: Menu bar: CNC .

Requirement: A CNC path is open in the editor. The CNC program is implemented as DIN66025.

If step suppression is activated, then blocks in the CNC program that begin with / are ignored.

If the CNC program is implemented as a table, then the command is not available.

See also