A gantry cutter is a gantry system with a rotary axis that is equipped with a cutting tool.
The configuration of a gantry system with a rotary axis is similar to that of a simple gantry system. However, these systems also have a rotary axis where the vertical cutting unit is attached.
When you use a gantry system with a rotary axis, you have to use the SMC_TRAFO<n>_GantryCutter<n>
POUs instead of SMC_TRAFO<n>_Gantry<n>
. Then, the rotary axis is controlled in such as way that it is oriented along the current path tangent.
The gantry cutter POUs have the following additional inputs:
DriveR
: Rotary axis that has to be used with a period of 360°
dOffsetR
: Offset of the rotary axis
iDirectionR
: Direction of rotation
See also
The POUs for inverse transformation also have to include the vector of the current path tangent (v) that is an output of the interpolator.
See also