Command 'Get lock'

Symbol:

Function: This command locks the object explicitly for you. The Lock Message dialog opens for this purpose.

Call: Context menu: SVN

Requirement: The versioned object is not locked (not overlaid with the symbol).

Dialog 'Lock Message'

Enter the reason why you lock the object:

Lock message

Example: Locked for processing task 123

Button Recent Message

Shows message in the dialog that have already been used. There you select one in order to use the lock message.

Recursive

: The object is locked with all subordinate child objects.

OK

Locks the object

When the lock is successful, the object (in the object tree) is overlaid with the symbol.