Command 'Compare'

Symbol:

Function: This command opens a tab that shows the result of the comparison of your working copy and the BASE revision. The base revision is the top-level revision in the SVN repository.

Call:

  • Menu bar: Project ‣ SVN .

  • Context menu

Requirement: The object is versioned, it was modified locally, and it does not contain any conflicts.

Multiple tabs can be open at the same time with the comparison of different objects.

Note

Comparison by object type The comparison dialog makes use of the functionality of the CODESYS command Project ‣ Compare . In this way, objects are compared according to their object type.

See also