Symbol:
Function: This command deletes all connections of the current project to SVN by converting the project into a non-versioned project.
Call: Menu bar:
.Because this operation cannot be reversed, the operation must be confirmed before the command is executed.
Use the command "Connect to existing project” to connect to the SVN repository again at a later time.
See also