Command 'SVN Repository Browser'

Symbol:

Function: This command opens the SVN repository browser. The contents of an SVN repository is shown in a tree structure here. You can search through the repository in the browser.

Call: Menu bar: Project ‣ SVN .

Depending on the selected object, the following commands are available in the context menu:

  • Show log

  • Checkout

  • Create folder

  • Copy to

  • Rename

  • Delete

Double-clicking the object with the right mouse button opens the log dialog.

Dialog 'SVN Repository Browser'

URL

URL in SVN repository

Example: https://svnserver/repository/trunk/ControlABC.project

Tip: As soon as a valid SVN repository is specified, you can browse and select a specific project by means of the adjacent button.

Opens the dialog Select revision.

The button is labeled with the currently selected revision:

  • HEAD: Top revision (latest). Preset

  • 3: Revision number of the selected revision

  • 23.12.2016 11:59:59 (UTC): Change date of the selected revision (UTC)

Note: The dialog provides the same options as the Revision group.

Updates the browser view by rescanning the SVN repository.

Navigates the URL address up by one folder.

Left area

Directory tree in the SVN repository. Project nodes are shown in bold.

Note: In this view, you can directly edit the project name and the name of the superordinate folder.

Right area

List of objects of the selected directory

Close

Closes the dialog

See also