Symbol:
SFunction: This command opens the Update dialog. In the dialog, the revision is defined for updating the project.
Call:
If you select nothing or the base node in the object tree, then the entire project is updated to a revision (Update project to revision). If you select one or more objects, then these objects are updated and their sub-objects are updated recursively (Update to revision). As an option, you can define that the sub-objects are not updated.
The behavior of the updating process (for example merging of conflicts) is similar to the Update project and Update commands.
HEAD |
|
Revision |
|
Date |
Use UTC time: |
Recursive |
|
Omit external objects |
|
See also