Tab 'EtherCAT Slave - Parameters'

Object: EtherCAT slave

This tab contains the slave parameters that are defined in the device description file.

If the auto-configuration mode of the master is activated, then the parameters are set automatically here in accordance with the specifications from the device description file and the network topology. For standard applications it is also normally not required to edit them.

Value

Only a few parameters are editable. Change is only effective if auto-configuration mode is deactivated.

In principle the user should not change anything here, since in doing so an invalid configuration could be created, thus preventing the slave from entering the operational state.