Library: IODrvEtherCAT
Like ETC_CO_SdoRead
, this function block is for reading EtherCAT slave parameters. The additional input xCompleteAccess
(BOOL
) enables the reading of the complete index with all entries. To do this xCompleteAccess
must be set to TRUE
and bySubIndex
must be 0
.
See also