ETC_CO_SdoRreadDword

Library:IODrvEtherCAT

Like ETC_CO_SdoRead4, this function block is for reading EtherCAT slave parameters. However, the data to be read are transferred not as an array, but in a DWORD (dwData). If byte swapping is necessary it is carried out automatically. The read value can thus be reused directly.

See also: