An instance of the ETCSlave
data type is generated for each EtherCAT slave inserted in the device tree. The name of the instance corresponds to the name of the slave in the device tree. The availability of the instance is displayed in the IEC Objects tab of the device editor.
The slave instance is used in the application in order to query or change the state of the slave at runtime.
Name |
Data type |
Description |
---|---|---|
|
|
Rising edge: An attempt is made to switch to the |
Name |
Data type |
Description |
---|---|---|
|
|
Current state of the slave:
If errors occur during the configuration, the slave can fall back into an earlier state. |
|
After the EtherCAT stack starts, this property returns the vendor ID that is read from the device. |
|
Reads the vendor ID from the configuration. |
|
After the EtherCAT stack starts, this property returns the product ID that is read from the device. |
|
Reads the product ID from the configuration. |
|
After the EtherCAT stack starts, this property contains the serial number of the device. |
|
If a message is received, this information is stored in the slave and can be queried from the application with this property. A log message is also added. |
If the checking of the vendor or product ID is activated in the expert settings, then the boot up of the stack is stopped as soon as a discrepancy is found between VendorID
and ConfigVendorID
or between ProductID
and ConfigProductID
.
See also