This tab can be used to read the parameters from the IO-Link device, to modify them and then to write them back to the device.
Refer to the following description for information about the tab of the device editor.
Tab 'IO-Link Parameters'