Function: The command displays the network topology of the PROFINET network as a tree structure. For each port of the PROFINET device, the neighboring device connected here and its port are displayed (if available).
Call: Context menu of a PROFINET controller.
Requirement: The communication settings to the controller are correct. The gateway and the PLC are running. The device supports the scan function.
|
Refreshes the view |
IM |
Gets the I&M data (identification and maintenance) of the device and view in a dialog |
Auto IP |
Automatic setting of a valid IP address for the selected device in case the address scanned by the device is invalid. |
Port State |
Possible states:
|
Neighbour |
Name of the neighboring device in the network. In the case that the device does not support the function or does not have a valid IP configuration, "No data!" is displayed. Details about the error cause are shown as a tooltip. |
Neighbour-Port |
Name of the neighboring port in the network. |
See also