Object: PROFINET Slave Device
The tab shows the diagnosis data of the slave device and the subordinate modules. For the slave device, additional status information about the driver is shown.
Diagnosis Data |
The diagnosis entries that are currently in the diagnosis database of the device for the selected module. The entries of this database can be created or deleted from the device application by means of the |
See also