CANopen Manager (Master)

In a CANbus configuration, the CANopen manager is a required node below the CANbus node. This manager is typically used as a CANbus master.

CODESYS provides the following CANopen managers:

  • CANopen Manager (1)

  • CANopen Manager SIL2 (2)

  • CANopen Manager SoftMotion: Can be inserted below a SoftMotion controller; contains adapted presets for a motion bus.

See also