Function: This command lets you switch between the CODESYS perspective and the HMI perspective.
Call: Menu bar:
.See also
|
CODESYS is displayed in the usual tree oriented perspective in which IEC applications are typically developed. |
|
CODESYS is displayed in the HMI perspective that supports the development of HMI applications. The perspective is subdivided into individual views: Visualizations, Data Sources, and HMI Features. |
See also