Command 'Reset to Default'

Function: The command resets the position value of the element within the Tab Order to the original value.

Call: Element list in the visualization editor; context menu in the Tab Order column

The Tab Order, which is defined in the element list, originally results from the order of the elements on the individual display layers of the visualization (numbering in the Type column). When positions have been changed (see the Move to Position command), they can be reset by means of the Reset to Default command. This is possible simultaneously for a multiselection of elements.

See also