Permissions for visualization-elements are not granted to individual users, but to groups with assigned users.
Requirement: A Visualization object is open with at least one inserted visualization element.
Click a visualization element in the editor.
Click the Value field of the Permissions element property in the Properties view.
⇒ The Permissions dialog box opens.
Select the permissions that the respective user group should have for the visualization element.
Note: If the option Group hierarchy is used is activated, the groups lower in the hierarchy cannot be granted more permissions than groups higher in the hierarchy.
In the Element List of the visualization, the Permissions column shows the element permissions granted to groups.
See also