Function: This dialog is used for creating a new object of type Visualization.
Call:
; context menu of an applicationRequirement: An application is selected in the device tree.
The following settings are displayed only when you add an object of type Visualization to the project for the first time. |
|
Symbol library |
List of all installed symbol libraries |
Assigned |
Tip: CODESYS manages this setting in the project settings. |
Add |
CODESYS creates a new visualization, assigns the selected symbol libraries to the project, and provides them in the ToolBox view. |
See also