Function: In this dialog box, you define the alarm groups that are considered for the alarm table or alarm banner.
Call: Property Alarm configuration / Alarm groups of the alarm table or alarm banner visualization element.
Requirement: An alarm table visualization element or alarm banner visualization element is added to the visualization.
Available Alarm Groups |
Shows all alarm groups created in the project. |
Selected Alarm Groups |
The alarm groups in this column are displayed in the alarm table. |
All |
|
|
Moves all available alarm groups to the Selected Alarm Groups column. |
|
Moves the selected alarm groups to the Selected Alarm Groups column. |
|
Removes the selected alarm groups from the Selected Alarm Groups column. |
|
Removes all alarm groups from the Selected Alarm Groups column. |
See also