You can execute the visualization as an integrated visualization. In this case a display variant of the visualization runs on the development system without the visualization code being loaded to the controller.
Use the integrated visualization for the testing and diagnosis of your application, or for the service and commissioning of a plant.
The requirement for this is that there are no objects under the visualization manager. Alternatively, any objects located there can be excluded from compilation. You can configure an individual object accordingly in its dialog Properties on the tab Build.
See also
In the case of projects with a fixed compiler version < 3.3.2.0
, the activation of the Don't use the PLC for Visu option is necessary in order to execute the visualization as an integrated visualization.
The option no longer exists for version 3.3.2.0
and later.
A visualization project is open.
Remove all objects from underneath the visualization manager or exclude the objects from compilation.
⇒ The VISU_TASK
has been removed from under the task configuration.
Download the application to the controller.
⇒ Now no visualization code will be transferred on loading the application.
Start the application.
⇒ The visualization in the visualization editor is being executed. You can operate your application.
Use the command Activate Keyboard Usage in order to toggle between the keyboard usage of the integrated visualization and the keyboard usage of CODESYS.
See also
Numerical variable values, which are output within a text in an integrated visualization, are displayed according to the current display format. You can select the display format with the command
.See also
A variable value that is transferred via the data source manager is not output. The integrated visualization only outputs the initialization or the last transferred value.
The integrated visualization thus only enables a passive observation of the application.
VAR_INPUT
variables behave like integrated visualizations such as VAR_IN_OUT
during execution.
Only the following expressions, which are also used in the monitoring mechanism of the development system, are supported in an integrated visualization.
Variable access:
Example: PLC_PRG.myPou.nCounter
Array access:
Requirement: The version of the runtime system is at least V3.3 SP2
or later.
Access to an array of scalar data types, where a variable is used as an index
Example: a[i]
Access to an array of complex data types (structure, function block, array), where a variable is used as an index
Example: a[i].x
Access to a multidimensional array of all kinds of data types with one or more variable indices
Example: a[i, 1, j].x
Access to an array with constant index
Example: a[3]
Accesses like those described above in which simple operators are used for the calculations inside the index brackets.
Example: a[i+3]
Nested combinations of the complex expressions listed above
Example: a[i + 4 * j].aInner[j * 3].x
Operators in index calculations:
+
, -
, *
, /
, MOD
Pointer monitoring:
Example: p^.x
Methods and function calls are not supported except for the following:
Standard string functions
Type conversion functions
Example: INT_TO_DWORD
Operators such as SEL
, MIN
, etc.
When the input action Execute ST code is called, only a list of assignments is supported.
If a list of assignments is used, the value of the left-hand side is not assigned until the next cycle. Processing in the next row immediately afterwards is not possible.