Symbol:
Function: With the object, the visualization is downloaded to the controller and the start visualization for the Remote TargetVisu is defined.
The object is added to the Visualization Manager of an application.
See also
Run as Remote TargetVisu