The 'Filter options' dialog appears after clicking the 'Filter' button in the event log dialogs. It is used to filter the present event log in order to show only a particular subset of entries.
The system event log can only be filtered for the 'User'.
Filter option |
Meaning |
---|---|
Log Events |
Only log-related events in the log are displayed (e.g., resets of the event log). |
Project Events |
Only project-related events in the log are displayed (e.g., insertion or deletion of libraries). |
POU Events |
Only POU-related events in the log are displayed (e.g., insertion or deletion of POUs). |
Device parameterization Events |
Only device parameterization-related events in the log are displayed (e.g., modifying the configuration of safety-related I/O devices). |
SafePLC Events |
Only error messages received from the Safety Logic Controller error stack are displayed. |
Bus Navigator Events |
Only Bus Navigator-related events are displayed (e.g., changing the Safety Logic Controller). |
User |
Only event log entries of this particular user are displayed. |