DecodeClass (FUN)

FUNCTION DecodeClass : EVENT_CLASS

This function serves to extract the vaue eClass of type EVENT_CLASS from parameter dwSpec of the callback function.

InOut:

Scope

Name

Type

Comment

Return

DecodeClass

EVENT_CLASS

The EVENT_CLASS of dwSpec.

Input

dwSpec

DWORD

A combination of EVENT and EVENT_CLASS