GET_CANOPEN_KERNEL_STATE (FB)

FUNCTION_BLOCK GET_CANOPEN_KERNEL_STATE EXTENDS CiA405Base

Gets the current state of the CANopen Kernel. As long as CANopen network is running correctly the function block returns CANOPEN_KERNEL_ERROR.CANOPEN_KERNEL_NO_ERROR for output STATE. The function block detects bus errors, configuration errors, guarding errors and internal system errors (e.g. out of system memory).

InOut:

Scope

Name

Type

Initial

Comment

Inherited from

Input

NETWORK

USINT

1

CAN network number the function block should operate on. Note: It is not the same like the network number in CANBus configurator. The CiA405 NETWORK is calculated by NetID + 1. Example: 1 = CAN0, 2 = CAN1, 3 = CAN2, ...

CiA405Base

ENABLE

BOOL

FALSE

Enables the function block on rising edge. Aborts operation on falling edge.

CiA405Base

TIMEOUT

UDINT

0

Timeout in ms; 0 means no timeout

CiA405Base

Output

CONFIRM

BOOL

FALSE

TRUE: function block finished without error

CiA405Base

ERROR

CANOPEN_KERNEL_ERROR

CANOPEN_KERNEL_ERROR.CANOPEN_KERNEL_NO_ERROR

Error code: see CANOPEN_KERNEL_ERROR for further details

CiA405Base

STATE

CANOPEN_KERNEL_ERROR

CANOPEN_KERNEL_ERROR.CANOPEN_KERNEL_NO_ERROR

Current stack state.