Function block returns the NodeID of the local device (= CANopenManager)
InOut:
Scope
Name
Type
Initial
Comment
Inherited from
Input
NETWORK
USINT
1
CAN network number the function block should operate on. Note: It is not the same like the network number in CANBus configurator. The CiA405 NETWORK is calculated by NetID + 1. Example: 1 = CAN0, 2 = CAN1, 3 = CAN2, ...
CiA405Base
ENABLE
BOOL
FALSE
Enables the function block on rising edge. Aborts operation on falling edge.