GetPos (FB; Prefix filgp)

FUNCTION_BLOCK GetPos EXTENDS CBM.ETrig

This function block returns the offset position currently set in the file. The file must be opened via FILE.Open.

InOut:

Scope

Name

Type

Comment

Input

hFile

CAA.HANDLE

File handle

Output

eError

ERROR

Local library error ID (0: no error; 5101: time out)

udiPos

__UXINT

Offset position; Number of bytes from the start of the file