The AS-i Gateway does not only enable the communication between SLC/LMC and the AS-i slaves, it may also implement control functionality by executing the AS-i application configured with the Bihl+Wiedemann configuration, programming, and diagnostic tool ASIMON. The use of ASIMON and the steps to adapt/develop the configuration project is not part of this documentation. Refer to the ASIMON documentation provided by Bihl+Wiedemann for information.
The user-definable mapping of safety-related AS-i data to the bits of the '8 Bytes Safe Sercos Data' device object has also to be done in ASIMON. These safety-related AS-i data are generated as follows: by means of a special, device-specific algorithm, the AS-i communication telegram of each connected safety-related AS-i slave is permuted into one safety-related data bit per AS-i slave. This safety-related data bit can be mapped to the '8 Bytes Safe Sercos Data' device object in ASIMON (see below). Standard (non-safety-related) AS-i slaves cannot be mapped to the device object.
The present documentation is predicated on the best practice of a 1:1 data mapping application. This means, the address of an AS-i slave corresponds to the input/output bit number in the '8 Bytes Safe Sercos Data' device object which is exchanged between the AS-i Gateway, SLC and LMC (via Sercos). AS-i slave 1 connected to AS-i circuit 1 is mapped to bit 1, AS-i slave 2 is mapped to bit 2, and so on.
Besides this straight 1:1 mapping, each user-definable mapping of AS-i data to the bits in the device object is possible. However, keep the mapping as clear as possible to help avoiding incorrect data assignments in the safety-related application.
In ASIMON, map each connected AS-i slave to the '8 Bytes Safe Sercos Data' device object. Use a straight 1:1 mapping.
In ASIMON, configure the application logic.
Implementing AS-i circuit diagnostics:
If configured in ASIMON, the AS-i Gateway provides diagnostic status signals for both AS-i circuits (similar to the SafeModuleOK signal from TM5/TM7 modules). These bits indicate the status of the respective AS-i circuit and of the communication between the AS-i Gateway and the SLC, and therefore, from safety-related application perspective, the AS-i Gateway status itself.
Make sure that ASIMON is setup in a way that the diagnostic status signals for the AS-i circuits 1 and 2 are generated and output.
Map the diagnostic status signals for the AS-i circuits 1 and 2 in ASIMON to the input bits 0 and 32 of the '8 Bytes Safe Sercos Data' device object. Input data bit 0 then represents the status of AS-i circuit 1, and input bit 32 represents circuit 2.
When developing the safety-related SLC application in EcoStruxure Machine Expert - Safety, you have to evaluate the input bits 0 and 32 in a way that the signals coming from the AS-i slaves are considered as invalid if the circuit status signal is SAFEFALSE. Refer to the topic "Reading and Writing AS-i Data Bits in EcoStruxure Machine Expert - Safety" for details. In particular observe the information given in section "Description of the AS-i input/output bits".
Implementing enable output signals to control the AS-i output circuits:
Use suitable Boolean output variables generated in the safety-related SLC application as enable output signals for each of the output AS-i circuits.
Map these enable output signals to the output bits 0 and 32 of the '8 Bytes Safe Sercos Data' device object.
Process the output bits 0 and 32 accordingly in the ASIMON application using logical AND combinations in a way that a slave may only activate its output if the enable signal is SAFETRUE.
In doing so, the output bits 0 and 32 of the '8 Bytes Safe Sercos Data' device object can be used for enabling the circuits 1 and 2 (similar to the ReleaseOutput signal known from TM5/TM7 modules). Setting an enable bit to SAFETRUE means that the related AS-i slaves may activate their outputs.
Refer to the topic "Reading and Writing AS-i Data Bits in EcoStruxure Machine Expert - Safety" for details. In particular, observe the information given in section "Description of the AS-i input/output bits".
Each modification in the AS-i application results in a newly calculated ConfigID value (see section below).
Each AS-i application is verified by a unique checksum which is generated in ASIMON before copying the configuration data to the AS-i Gateway and commissioning the AS-i application. In ASIMON, this checksum is called ConfigID.
Each modification in the AS-i application results in a newly calculated unique ConfigID.
In EcoStruxure Machine Expert - Safety, this ConfigID has to be entered as safety-related 'ConfigID' parameter in the Device Parameterization Editor. This checksum is used to verify that the configuration and application loaded in the AS-i Gateway is valid and corresponds to the AS-i configuration entered in EcoStruxure Machine Expert - Safety.
Refer to the ASIMON documentation, how to determine the ConfigID checksum value.
(Also observe the possibility of displaying the ConfigID at the device as described below.)
Note down the ConfigID generated by ASIMON. It has to be entered as 'ConfigID' parameter in EcoStruxure Machine Expert - Safety.
You can also display the ConfigID at the AS-i Gateway device. Press the 'OK' button at the device to enter the menu and select 'Safety > Safe Sercos > Config IDs (Node and Manager)' to display the ConfigID.
The 'Node' entry on the displayed screen outputs the ConfigID configured on the AS-i Gateway device.
The 'Manager' entry displays the ConfigID which is entered in the safety-related device AS-i Gateway parameters in EcoStruxure Machine Expert - Safety.
If the value is 0, either no communication connection is established between EcoStruxure Machine Expert - Safety and the AS-i Gateway, or communications will be unsuccessful because of the invalid ConfigID.